Change the background color of a screen

Change the background color of a screen to a different color, gradient color, or custom color.
To change the background color of a screen:
  1. In the
    Project Explorer
    , expand the
    User-Defined Screens
    or
    Predefined Screens
    folder.
  2. Select the screen, or double-click the screen to open it.
  3. In the
    Properties
    window, select the
    Properties
    tab.
  4. Expand the
    Appearance
    category.
  5. In the
    FillColor
    box, select a color using one of these methods:
    • In the
      Color Picker
      , create a color gradient.
      The selected color appears in the
      Fill Color
      box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal