Synchronization between the runtime application and the controller

When downloading the HMI project to the HMI device, the synchronization service connects the runtime application to the controller referenced in the HMI project. After the synchronization service connects to the controller, it reads data from the controller to determine if it matches the data in the HMI project. If the data does not match, the data in the HMI project automatically synchronizes with the data in the controller.
When the runtime application runs on the HMI device, the synchronization service checks if the
Logix Designer
file in the controller was updated. The
Logix Designer
project file in the controller can be updated using the online editing features in
Logix Designer
. If the project file was updated, the synchronization service will automatically synchronize data between the
Logix Designer
project file referenced in the runtime application and the newly updated
Logix Designer
project file in the controller.
Configure system tags to display information about the synchronization status of the runtime application and the Logix5000 controller or use the ControllersGeneral screen in the
Predefined Screens
folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal