Synchronization: Controller state indicator icons
These are the controller state indicator icons:
Icon | Description |
A controller is synchronizing. | |
The data in a controller is not synchronized. Controller data synchronizes automatically. Hover the mouse on the icon to display additional information. | |
A synchronization error occurred. The Logix Designer project file (.acd) does not exist, or it is a version that is not supported. Hover your mouse on the icon to display additional information. | |
The controller is synchronized. |
Provide Feedback