What is the Alarm Summary?
The
Alarm Summary
lists alarms that are In Alarm or Unacknowledged. The Alarm Summary
automatically subscribes to all alarms from the controller references specified in the project properties. It displays one alarm condition per row. Use the Alarm Summary
to monitor and interact with alarms. Add or remove columns to show different data for alarms in the Alarm Summary
table. Use the
Alarm Summary
on an HMI device to: - Acknowledge alarms.
- Disable alarms.
- Shelve alarms.
- Sort alarms.
- Filter alarms.
- Pause alarms.
- Reset digital alarms.
- View alarm details.
Provide Feedback