Predefined Screens folder

The
Predefined Screens
folder in the
Project Explorer
contains default screens, popups, and a
Banner
item for each project. The contents of the
Predefined Screens
folder includes:
  • Banner.
    By default, this item appears at the top of each project screen. It displays date and time, active and unacknowledged alarm indicators, controller diagnostic, and network diagnostic information. It also provides buttons to navigate to the
    Alarm Summary
    , log on and log off the project, move backward and forward through navigation history, and display the
    Navigation menu
    at the bottom of the HMI device.
  • Settings.
    This screen provides a menu to configure settings for the HMI device. By default, access the
    Settings
    screen through the
    Navigation menu
    on the HMI device. The options on the
    Settings
    screen open the popups listed under the screen in the
    Predefined Screens
    folder. These popups perform tasks to configure HMI device settings.
  • AlarmSummary.
    This screen displays the
    Alarm Summary
    , a list of alarms that are in interestingstates or that require attention. For example, the
    Alarm Summary
    lists alarms that are In Alarm and Unacknowledged. By default, access the
    AlarmSummary
    screen through the System Banner or the
    Navigation menu
    on the HMI device.
  • AlarmManager.
    This screen displays the
    Alarm Manager
    , a list of all alarms regardless of their state. Alarms listed in the
    Alarm Manager
    include all of the conditions for an alarm. By default, access the
    AlarmManager
    screen through the
    Navigation menu
    or the
    Alarm Summary
    on the HMI device.
  • AlarmHistory
    . This screen displays the
    Alarm History
    , a list of all alarm state changes. By default, access the
    AlarmHistory
    screen through the
    Navigation Menu
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal