Remove a graphic element from the System Banner

Remove a graphic element from the
System Banner
to no longer show that item at the top of each screen and shortcut in a project.
To remove a graphic element from the System Banner
  1. In the
    Project Explorer
    , expand the
    Predefined Screens
    folder.
  2. Double-click the
    Banner
    item. The
    System Banner
    opens.
  3. Select the graphic element on the
    System Banner
    and press
    Delete
    . The graphic element no longer appears on the
    System Banner
    . Removing a graphic element from the
    System Banner
    does not remove the item from the
    Toolbox
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal