Open the System Banner

Open the
Banner
item to add or change the contents of the
System Banner
. The
System Banner
contains default items.
To open the System Banner
  1. In the
    Project Explorer
    of the open project, expand the
    Predefined Screens
    folder.
  2. Double-click the
    Banner
    item. The
    System Banner
    opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal