Copy and paste a graphic element on the System Banner
Copy and paste graphic elements in the
System Banner
to repeat a graphic element at the top of each screen in the project. Configure copied graphic elements with different property values, animations, or events like any other graphic element. When copying and pasting graphic elements in the System Banner
, leave space between items to make them more easily tapped on the HMI device. To copy and paste a graphic element on the System Banner
- In theProject Explorer, expand thePredefined Screensfolder.
- Double-click theBanneritem.
- On theSystem Banner, right-click the item and selectCopy.TIP:To select multiple items, holdCtrland select the items.
- Right-click anywhere on theSystem Bannerand selectPaste.
- Drag the graphic element to the desired position on the banner rectangle.
Provide Feedback