Export Languages dialog box
How do I open the Export Languages dialog box?
On the
Menu
bar, click Tools > Export Languages
.Use the
Export Languages
dialog box to export user-editable text strings in a project so that the strings can be translated. View Designer
creates a language file that contains all of the strings used in the project along with their location within the project. Use the
Export Languages
dialog box to:- Specify the default language of the project.
- Select the languages for translation.
- Select the location to save the exported language file.
Provide Feedback