VNC tab
How do I open the VNC tab?
On the
Menu
bar, click Tools > Security Administration
, and on the Security Administration
dialog box, click the VNC
tab.VNC is a protocol used for remotely connecting to an HMI device. Use the
VNC
tab on the Security Administration
dialog box to configure or change access rights for users remotely connecting to an HMI device. The available access rights are View-Only and Full-Control. Provide Feedback