Security for HMI devices

Access to the HMI device is either through user name and password or PIN.
Set up user accounts to access the HMI device on the
Security Administration
dialog box. Assign each user a password and/or PIN. Use the
Policies
tab on the
Security Administration
dialog box to create security policies such as password complexity and length and to enforce password strength.
Use the Guest user account to restrict users that do not log in. Have the Guest user view only the Home screen or certain screens.
The
HMI Device
screen in the
Predefined Screens
folder provides a way to prevent overwriting the runtime application in the HMI device. Clear
Allow Downloads
and
Firmware Updates
to prevent downloading a project or updating firmware on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal