Restrict access to the HMI device
Restrict access to the HMI device by selecting a method for users to log on to the HMI device:
To restrict access to the HMI device
- On theProject > Project Properties > Log On Methodtab, select a Security option:
- Use user name/password for logging on
- Use PIN for logging on
- On theTools > Security Administration > Userstab, enter a password or PIN for each user.
- (optional) On theSecurity Administration > Policiestab, adjust the complexity requirements for passwords by specifyingPassword Policy Settings:
- Log off the user after a period of inactivity.Set in minutes how long the user has to remain inactive to be automatically logged out.
- Minimum password length. Specify the minimum amount of characters required. The maximum number allowed is 14.
- Password history. Type the number of previous passwords to remember. This enforces a password history and sets how frequently you can reuse old passwords. The maximum number allowed is 24.
- To disable this feature, set theNumber of Passwords to Rememberto zero.
- Passwords must meet complexity requirements.Select this option to enforce complexity requirements when you create or change passwords.TIP:Passwords that meet complexity requirements must:
- Not contain the User Name.
- Not contain any portion of the Full Name.
- Contain characters from three of four categories:
- Uppercase characters of European languages (A through Z, with diacritic marks, Greek and Cyrillic characters)
- Lowercase characters of European languages (a through z, sharp-s, with diacritic marks, Greek and Cyrillic characters)
- Numbers 0 through 9
Non-alphanumeric characters ~!@#$%^&*_-+=`|\(){}[]:;"'<>,.?/
Provide Feedback