Restrict access to settings on the HMI device
By default, any user not logged into the project on the HMI device has Administrator access to the Settings screens. These screens in the
Predefined Screens
folder of the Project Explorer
configure the HMI device at runtime. Limit the access guest users have to the Settings screens by assigning any role but the Administrator
role. Users who are not assigned the Administrator have Read Only access to the Settings screens. This prevents non-Administrator users from disrupting the system. For example, a Guest user cannot reboot the HMI device. The user can still navigate to and open all of the Settings screens on the HMI device to review the HMI device settings and configuration. To restrict access settings on the HMI device
- SelectTools > Security Administration. TheSecurity Administrationdialog box opens.
- In theGuest Userbox afterRole, select any role, includingNone, that is not theAdministratorrole.All options on the Settings screens on the HMI device are Read Only for any user except an administrator.
Provide Feedback