Restrict access to a graphic element

Restrict access to a graphic element to allow or disallow touch events. For example, prevent users from navigating to a screen in the project.
To restrict access to a graphic element
  1. Select the graphic element on the screen.
  2. In the
    Properties
    window, expand the
    Security
    category.
  3. In the
    Access
    property box, select a security level from the list:
    • Inherit
      (default). The security level of the screen determines if the graphic element is enabled or disabled. Graphic elements that support cross-hatching when they are disabled display with cross-hatching.
    • Full Access
      . The security level of the screen is ignored and the state of the
      Enabled
      property for the graphic element is used to determine if the graphic element is enabled or disabled, and displays with cross-hatching.
      TIP:
      If the
      Enabled
      property check box for the graphic element is cleared, the graphic element is disabled and shows cross-hatching regardless of the
      Security Access
      property setting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal