Log on using network-based security
To log on using network-based security:
- To log on to the application using your network-based security configuration, on the top of the screen, select the log on button
.IMPORTANT:The user name used for theUser Principal Namemust be used during Active Directory logon. - Ensure that you are logging on as a domain user, enter your Active Directory user name and password, and SelectLog on.

IMPORTANT | When StartTLS or LDAPS encryption method is configured, you are required to import the proper security certificate to the terminal by using the Certificates setting screen. A caching mechanism is used for users who successfully logged on with Active Directory authentication. If the PanelView 5000 loses connection to the Active Directory, the user can still log on with cached domain credentials for 24 hours. After this period, logon is no longer possible without an Active Directory connection. The Cache is only cleared on project download, and not on reboot or restart. |
![]() | Tip: You can switch between a local user and a domain user by selecting the link at the bottom of the Logon screen.If the Connection information is left blank in View Designer , only local user logon will be used by the logon dialog at runtime. |
See also
Provide Feedback