Delete ports from the list of open ports
Remove ports from the list of open ports to no longer have the port open on the HMI device.
TIP:
This function is not available for
View 5000 Server
. Use Windows
to configure ports.To delete ports from the list of open ports
- SelectTools > Security Administrationand select thePortstab.
- Select a row in the in the table. To select multiple rows, holdCtrlwhen selecting.
- PressDelete.
- SelectOKto save the changes and close theSecurity Administrationwindow.
Provide Feedback