Add ports to open ports list
Add ports to the list of open ports to allow the HMI device to communicate with devices and web services that use specific ports. Add a maximum of 1000 ports.
TIP:
This function is not available for
View 5000 Server
. Use Windows
to configure ports.To add ports to the list of open ports
- SelectTools > Security Administrationand select thePortstab.
- Select
Add ports to open. The focus automatically moves to the new list row. - Enter a port number (1-65535) in thePortlist.
- SelectOKto save the changes and close theSecurity Administrationwindow,or select
Add ports to opento continue adding ports.
Provide Feedback