Add locations to the allowed locations list
Add URLs to the allowed locations list to grant users access to external resources through the Web Browser. The locations can be network locations, or files and folders on the removable media inserted in the HMI device. If the HMI device has multiple USB drives inserted, the drive inserted last is accessible. Add a maximum of 1000 locations. By default, the web browser blocks access to all locations not included on the allowed locations list. Add access to all servers used by the webpages that you add to the allowed locations list. Set access for different security roles.
To add locations to the allowed locations list
- SelectTools > Security Administrationand select theWeb Contenttab.
- SelectAdd URL
. Focus sets on the new table row. - Enter an URL using one of these schemes:
- http://
- https://
- ws://
- wss://
- sd:/
- usb:/
- (optional) use a scheme with an IP address or a ranges of IP addressesTIP:Tips:
- Use the asterisk * to substitute a character or a string of characters.
- Enter a single asterisk in the row to allow the security role to access all possible URLs.
- Enter*://and an IP address to access a location that may use HTTP or HTTPS protocol.
- Enter the schema without the rest of the URL to grant roles access to all locations using this schema.
- When entering a range of IP addresses, place the range in parentheses, for example: http://1.1.1.(5-158) or use asterisk to represent all values in a decimal (0-255): https://1.1.1.*.
- Select the security roles to access to the URL. By default, all roles are selected.
- SelectOKto save the changes and close theSecurity Administrationwindow, or selectAdd URL
to add additional locations.
Provide Feedback