Raster images look unclear in
View Designer

Raster images, such as .bmp, .tif, .jpg, or .png files, are comprised of a grid of pixels, or a bitmap. Scaling elements in
View Designer
to match the DPI of the HMI device so that fonts look correct on the HMI device can make raster images look unclear in
View Designer
. This happens when the DPI of the target HMI device is much larger than the DPI under which
View Designer
is running.
The unclear or pixelated effect occurs because the size of all of the elements on the screen are reduced to match the fewer number of pixels used to display fonts on
View Designer
. The image may look unclear in
View Designer
, but it displays correctly on the target HMI device. You can typically scale down raster graphics with little loss of quality.
Copying and pasting an image between
View Designer
projects for different size HMI devices maintains the physical size of the image. The image no longer has the same number of pixels on the new HMI device as it had on the original HMI device. Add the image to the new screen or manually resize the image to correct the size on the new HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal