Property Definition tab
How do I open the Property Definition tab?
The
below the screen to display the
Property Definition
tab is located below the Screen
area. Click Expand
Property Definitio
n tab if it is not open.The
Property Definition
tab contains the properties you create for the current screen, popup, or Add-On Graphic definition. Create a user-defined property to act as a placeholder for a value or data on a screen, Add-On Graphic definition, or popup. This enables you to use a screen multiple times by passing different values to the user-defined properties using a shortcut or navigation command. Using custom properties in
View Designer
increases the time it takes PanelView
5000 HMI devices to synchronize with changes to the controller program. When using custom properties in View Designer
, expect increased synchronization time when downloading a revised controller program to the controller or making online changes to the controller program.Use the
Property Definition
tab to create, change, or delete a user-defined property.Provide Feedback