Delete a user-defined property
Deleting a user-defined property deletes it from the project and all commands or screen shortcuts with which it is associated.
To delete a user-defined property
- Select the screen, popup, or Add-On Graphic definition that contains the user-defined property.
- In theProperty Definitiontab below the open screen, select the box to the left of the property.
- To select all of the properties in the table, selectSelect All
.
- Right-click and selectDelete Selected Row(s).
Provide Feedback