Copy an image assets folder
Copy an image assets folder to add the image to the
Images
folder and make it part of the target project. To copy an image assets folder
- In theProject Explorerof the source project, open theImagesfolder located in theAssetsfolder.
- Right-click the image and selectCopy.
- In theProject Explorerof the target project, expand theAssetsfolder.
- Right-click theImagesfolder and selectPaste.
Provide Feedback