User-defined alias property for an Add-On Graphic
In this example, alias properties in the definition of an Add-On Graphic appear on each instance of the Add-On Graphic. Entering a value or binding changes the value of the aliased property on an instance of the Add-On Graphic.

Add-On Graphic definitionItem | Description |
![]() | The alias property. In this example, the alias is for the LevelColor. Create an alias property by right-clicking the property and selecting New Alias . The alias property appears in the Property Definition tab below the definition of the Add-On Graphic. |
![]() | The user-defined alias property for the definition of the Add-On Graphic:
|
Add-On Graphic instancesItem | Description |
![]() | The Properties window for the first instance of the Add-On Graphic on a screen. The BeverageColor alias property for Mixer_001 is set to orange and appears orange on the HMI device. |
![]() | The Properties window for the second instance of the Add-On Graphic on a screen. The BeverageColor alias property for Mixer_002 is set to purple and appears purple on the HMI device. |
Provide Feedback