Add-On Graphics on reusable screens
This example depicts an Add-On Graphic with a mixer and a screen with additional mixer graphic elements. To have the screen and the Add-On Graphic on the screen show the values for the same mixer, bind the user-defined data type property that appears on an instance of the Add-On Graphic to the user-defined data type property of the screen. When a shortcut or navigation command passes a value into the user-defined property of the screen, graphic elements in the Add-On Graphic and on the screen show values from the same mixer. A Mixer1 shortcut or popup shows the values of Mixer1, and a Mixer2 shortcut or popup shows the values of Mixer2.

Add-On Graphic definitionItem | Description |
![]() | Graphic elements in the definition of the Add-On Graphic. |
![]() | A user-defined data type property named MixerTag in the Property Definition tab of the Add-On Graphic definition. |
![]() | The Properties windows for graphic elements in the definition of the Add-On Graphic. The value of each graphic element is bound to a member of the MixerTag data type in the user-defined property using the format PropertyName.MemberName. For example, the mixer graphic element is bound to MixerTag.Level and the input graphic element is bound to MixerTag.LevelSP. Search for user-defined data type properties created for the definition of an Add-On Graphic and the members of that property through the Tag Browser . |
Reusable screenItem | Description |
![]() | A screen containing an instance of the Add-On Graphic. |
![]() | A user-defined data type property named MixerTag created in the Property Definition tab of the screen. |
![]() | The Properties window of the selected instance of the Add-On Graphic on the screen. The Add-On Graphic is bound to the MixerTag user-defined data type property of the screen. |
HMI deviceItem | Description |
![]() | The binding of a shortcut to the Mixer1 instance of the controller tag. This binding passes the value of the user-defined property from the shortcut to the screen. On the HMI device, the graphic elements on the screen and on the Add-On Graphic show the values for Mixer1. |
![]() | The binding of a navigation command to the MixerTag user-defined property of the screen. This binding passes the value of the user-defined data type property to the screen when the event occurs. When the popup opens on the HMI device, the popup shows the values of Mixer1. |
Provide Feedback