Delete a folder
Delete a folder to remove it from the
Project Explorer
. When you delete a folder from the Navigation Menu
folder or User-Defined Screens
folder, the content of the folder is removed. Deleting the root level project is not allowed. Deleting certain folders is also not allowed: - Folder that contains theHomescreen
- Folder that contains screens with existing shortcuts
- Default folder --Navigation Menu,User-Defined Screens, orPredefined Screens.
To delete a folder
- In theProject Explorer, expand theNavigation Menufolder or theUser-Defined Screensfolder.
- Right-click the folder and selectDelete. The folder no longer appears in theProject Explorer. If you delete the folder from theNavigation Menufolder, the folder no longer appears on theNavigation menuon the HMI device.
Provide Feedback