Create a folder
Organize the contents of a project by creating folders in the The structure in the
Project Explorer
. For example, create a folder in the User-Defined Screens
folder to contain screens, popups, and other folders. Create a folder in the
Navigation Menu
folder to contain shortcuts and other folders. Create up to three levels of folders, including two levels of subfolders.Navigation Menu
folder of the Project Explorer
is depicted in the Navigation menu
on the HMI device.To create a folder
- In theProject Explorer, right-click theNavigation Menufolder. You can create a folder in theUser-Defined Screensfolder or a subfolder of the folder.
- ClickNew Folder. A new folder appears at the bottom of the folder with the default name Folder_001 or increment number. Folders at the same level must have unique names.
Provide Feedback