Change the position of the navigation menu

In station projects, you have an option to choose between a bottom or side menu. By default, the projects are uploaded with the side menu.
To set the side navigation menu:
  1. In the
    Project Explorer
    , select
    Navigation Menu
    .
  2. In the
    Properties
    section, select the
    Navigation Menu
    section.
  3. From the
    Menu Location
    drop-down menu, select
    SideMenu
    or
    BottomMenu
    .
  4. (optional for the side menu) In the
    Width
    section, set the width of the menu.
    TIP:
    You can select the values between 150 and 500 to set the width of the side menu.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal