Add a data log to a project

Add a data log to a project to create a log of specified tag values. Data logs collect data at a specific sample rate and for a specified duration. The data log collects data in the background when a project with a configured data log is running on the HMI device. Add up to three data logs to a project.
To add a data log to a project
  1. In the
    Project Explorer
    , navigate to the
    Data Logs
    folder.
  2. Right-click the
    Data Logs
    folder and select
    New Data Log
    . The initial data log added to a project has the default name DataLog_001.
    TIP:
    Tips:
    • Rename the data log through the
      Properties
      window.
    • Double-click the data log to open the data log. From an open data log change the sample rate, change the log duration, and add tags.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal