Close the Emulator
Close the
View 5000 Emulator
window to stop emulating the open project. To close the Emulator
- Perform one of the following to close the Emulator:
- Select
in the View 5000 Emulatorwindow. - Close the openView Designerproject.
- CloseView Designer.TIP:Tips:
- Running the emulator for two hours automatically closes the Emulator.
- Before the Emulator closes automatically after two hours, a banner below the title bar of theView 5000 Emulatorwindow indicates that the Emulator closes in five minutes.
Provide Feedback