Download a runtime application to a different HMI device
The screens in a project represent the physical size of the HMI device selected for the project.
How and if the screens are scaled to fit the new HMI device is based on the scaling mode you select in the following procedure.
To download a runtime application to a different HMI device
- Open the project.
- On theMenubar, selectProject > Project Properties.
- On theProject Propertiesdialog box, click theApplicationtab.
- In theScreen Scalingsection, select a scaling option:
- Scale with fixed aspect ratio.(Default) When you resize the screen, content is resized to fill the screen as much as possible while maintaining the same aspect ratio. If the aspect ratio of the screens changes from regular (4:3) to wide, or vice versa, squares and circles do not elongate into rectangles and ellipses.
- Stretch to fit.Resizes the screen content to fill the screen. As you resize the screen from wider or narrower and vice versa, squares and circles are elongated into rectangles and ellipses.
- Do not scale.Keeps the screen content the same size and position on the new HMI device as the original screens.
If the screen on the new HMI device is smaller than the original screen, the selected scale mode is overridden toThis assumes that Windows is calibrated to the DPI of the monitor on whichView Designeris running.Stretch to fitto ensure that no screen content is clipped off.
- ClickOKto save changes and close theProject Propertiesdialog box.
- From theMenubar, clickCOMMUNICATIONS>Download.
- In theLocationbox, clickBrowse
and select the IP address of the HMI device to which the runtime application is to download.TIP:Valid locations include View 5000 servers. - ClickNextto proceed to theController Referencespage.IMPORTANT:
- Projects are optimized for screen performance and text accuracy for the HMI device for which they are configured. Although projects can be downloaded to and displayed on any HMI device, there may be a speed and text size difference between HMI devices.
- When downloading a project or flashing an HMI device that has the screen saver running, the progress may not be visible. Stop the screen saver on the HMI device before beginning the download or flash process.
Provide Feedback