Specify the visibility of Automatic Diagnostics or Automatic Diagnostics History table

Specify if an automatic diagnostics table is always visible on the HMI device screen.
To specify the visibility of a table
  1. On the screen, select the
    Automatic Diagnostics
    or
    Automatic Diagnostics History
    table.
  2. In the
    Properties
    window, click the
    Properties
    tab.
  3. Expand the
    Appearance
    category.
  4. In the
    Visible
    box, select an option:
    • Visible
      (selected)
    • Not visible
      (cleared)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal