Specify the default sort order of Automatic Diagnostics or Automatic Diagnostics History table contents

Determine how table content is initially sorted on the HMI device screen. Specify which columns to sort and in which order, and whether to sort the contents of a column in ascending or descending order.
To specify the default sort order of table contents
  1. On the screen, select the
    Automatic Diagnostics
    or
    Automatic Diagnostics History
    table.
  2. In the
    Properties
    window, select the
    Properties
    tab.
  3. Expand the
    Appearance
    category.
  4. Enter columns and their order, in the
    SortOrder
    box
    • A valid column number, colon, and a D for descending or A for ascending. For example, 1:D,2:D provides a primary sort of Column 1 in descending order, and a secondary sort of Column 2 in descending order. You can enter a value for each column in the table.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal