Change the opacity of Automatic Diagnostics or Automatic Diagnostics History table
Change the opacity level of a table to adjust the transparency.
To change the opacity of a table
- On the screen, select theAutomatic DiagnosticsorAutomatic Diagnostics Historytable.
- In thePropertieswindow, click thePropertiestab.
- Expand theAppearancecategory.
- In theOpacitybox, enter a percentage, where 0 is fully transparent and 100 is fully opaque.
Provide Feedback