Help popup
The
on an HMI device. This popup shows a legend of icons that appear on the automatic diagnostics screens and the task each button on an automatic diagnostics table performs. The functions vary depending on the selected diagnostics table.
Help
popup opens when pressing Help
on an HMI device. This popup shows a legend of icons that appear on the automatic diagnostics screens and the task each button on an automatic diagnostics table performs. The functions vary depending on the selected diagnostics table.Help popup for Automatic Diagnostics table:

Help popup for Automatic Diagnostics History table:

Item | Description | |
|---|---|---|
![]() | Help popup. | |
![]() | A legend for automatic diagnostics functions you can perform on the automatic diagnostics table.The functions you can perform vary depending on the selected automatic diagnostics table: | |
![]() | Active, Unsuppressed displays the default state in which the message appears for the first time. This state informs that a fault occurs and requires immediate action. | |
![]() | Active, Suppressed displays the state in which the fault still exists. This state has already been viewed and suppressed by the user, so it may not require immediate attention, | |
![]() | Inactive, Unsuppressed indicates that the fault does not occur and that diagnostics are not in suppressed state. The fault appears only in the historical diagnostic data regarding fault resolution time. | |
![]() | Inactive, Suppressed displays that the fault no longer exists, but the diagnostics remains in the list until an Unsuppress operation is performed, usually without maintenance intervention. | |
![]() | Details hides or displays the Details pane, which contains the details of the last selected automatic diagnostics state change record. The Details pane replaces the list of diagnostics in medium automatic diagnostics tables. If no record is selected, the Details pane is empty. | |
![]() | Select All selects all of the diagnostics in the automatic diagnostics table, including those diagnostics displayed on the current page of diagnostics. | |
![]() | Deselect All deselects all diagnostics in the automatic diagnostics table, including those diagnostics displayed on the current page of diagnostics. | |
![]() | Select Page selects all of the diagnostics on the current page of diagnostics. | |
![]() | Suppress places the diagnostics event in the suppressed state. | |
![]() | Unsuppress places the diagnostics event in the unsuppressed state. | |
![]() | Refresh loads the latest automatic diagnostics state changes from the automatic diagnostics history. To display the latest state changes, close and reopen the Automatic Diagnostics History viewer. | |
![]() | Help opens the Help popup. This popup displays a legend of icons and the task each button on a diagnostics table performs. | |
Provide Feedback