Create an Automatic Diagnostics screen

Create an
Automatic Diagnostics
screen to view
Rockwell Automation
hardware diagnostics on the HMI device.
Automatic Diagnostics
screens receive diagnostics data automatically. There is no configuration required in
View Designer
.
By default, an
Automatic Diagnostics
screen and an
Automatic Diagnostics History
screen are included in the
Predefined Screens
folder of each
Project Explorer
for each project. When creating a custom automatic diagnostics screen, make the automatic diagnostics table the only graphic element on the screen. Do not add an automatic diagnostics table to a popup or the
System Banner
. Add an automatic diagnostics table to a screen only.
To create an Automatic Diagnostics screen
  • In the
    Automatic Diagnostics
    category of the
    Toolbox
    , drag and drop the automatic diagnostics table graphic element onto the screen.
    TIP:
    Tips:
    • Change the appearance of an automatic diagnostics table in the
      Properties
      pane. For example, to ensure an automatic diagnostics table contains readable content and has a row height that you can tap on the HMI device, change the font size and padding of the table cells. For an
      Automatic Diagnostics
      , change the number and content of columns.
    • Select filters to return automatic diagnostics meeting filter criteria on
      Automatic Diagnostics
      screen on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal