Automatic Diagnostics statuses

Automatic Diagnostics tables display 4 diagnostics statuses:
  • Active, Unsuppressed
    that shows the default state where the message appears for the first time. This state informs that a fault is present and requires immediate action.
  • Active, Suppressed
    shows the state where the fault still exists, but it has already been noticed and suppressed by using the
    Suppress
    command, so it may not require immediate intervention. This is useful for control system equipment which is under maintenance to temporarily ignore the faults from that equipment.
  • Inactive, Suppressed
    shows that the fault no longer exists, but the diagnostics remains in the list until an
    Unsuppress
    operation is performed, usually without maintenance intervention.
  • Inactive, Unsuppressed
    shows that the fault does not occur and the diagnostics is not in suppressed state. It appears only in the historical diagnostic data for information about fault resolution time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal