Create an HMIBC Button
Create a high-speed HMIBC button in an HMI project to initiate machine control operations, such as jogging a motor, with a high-degree of precision and determinism.
Any graphic element can be configured to function as a high-speed HMIBC button. Each Logix controller can support up to 256 HMIBC tags.
TIP:
The HMI Button Control (HMIBC) function is disabled for
View 5000 Server
projects.Provide Feedback