View the default content of a project

The
Predefined Screens
folder in the
Project Explorer
contains default screens, popups, and a
Banner
item for each project.
To view default content of a project
  1. Select
    View > Project Explorer
    .
  2. View the contents of the
    Predefined Screens
    folder:
    • Banner.
      Appears at the top of each project screen. It displays date and time, active and unacknowledged alarm indicators, controller diagnostic, and network diagnostic information. It also provides buttons to navigate to the
      Alarm Summary
      , log on and log off the project, move backward and forward through navigation history, and display the
      Navigation menu
      at the bottom of the HMI device.
    • Settings.
      Provides a menu of options to configure settings for the HMI device. By default, access the
      Settings
      screen through the
      Navigation menu
      on the HMI device. The options on the
      Settings
      screen open the popups listed under the screen in the
      Predefined Screens
      folder. These popups perform tasks to configure the HMI device.
      TIP:
      Restrict access to the screens that configure the HMI device. Apply any role that is not
      Administrator
      to the
      Guest User
      on the
      Security Administration
      screen. Any non-Administrator user, including users with the
      None
      role assigned, can open the popups but cannot change the options.
    • AlarmSummary.
      This screen displays a list of alarms that are in "interesting" states or that require attention. For example, the
      Alarm Summary
      lists alarms that are In Alarm and Unacknowledged. By default, access the
      AlarmSummary
      screen through the System Banner or the
      Navigation menu
      on the HMI device.
    • AlarmManager.
      This screen displays a list of all alarms regardless of their state. Alarms in the
      Alarm Manager
      include all of the conditions for a given alarm. By default, access the
      AlarmManager
      screen through the
      Navigation menu
      or the
      Alarm Summary
      on the HMI device.
    • Alarm History.
      This screen displays a list of all alarm state changes. Each row in the table contains one state change. By default, access the
      Alarm History
      screen through the
      Navigation menu
      on the HMI device.
      TIP:
      • To add or remove information and functionality from predefined items, change the content of predefined screens, popups, and the
        Banner
        item like any other screen. Do not remove content that configures the HMI device.
      • To restore the default content of a predefined screen, popup, or the
        Banner
        item, remove any remaining content from the revised item, open an unchanged version of the item in another project, and copy and paste the default content to the item.
      • Dragging the
        Settings
        ,
        AlarmSummary
        , and
        AlarmManager
        screens to the
        Navigation Menu
        folder in the
        Project Explorer
        creates a shortcut for the screen. The shortcut appears in the
        Navigation Menu
        . By default, these items are already in the
        Navigation Menu
        .
  3. View the contents of the
    Assets > Add-On Graphics
    folder:
    • PDF_Reader.
      This predefined Add-On Graphic occupies the entire screen of an HMI device to display, zoom, and navigate a PDF document.
    • PDF_Reader_Small.
      This predefined Add-On Graphic occupies half of the screen of an HMI device to display, zoom, and navigate a PDF document. This Add-On Graphic is not available on six-inch or seven-inch HMI devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal