Save Runtime Application wizard
How do I open the Save Runtime Application wizard?
- ClickFile > Save Project Asand navigate to a SD card or USB drive on which to store the runtime application.
- In theFile namebox, type a unique name for the runtime application.
- In theSave as typebox, selectView Designer Runtime Application (.vpdr)and clickSave.
Use the
Save Runtime Application
wizard to:- Save a runtime application .vpdr file to removable media.
- Select the default language of the .vpdr file.
- Download a project to an HMI device without usingView Designer.
After saving the runtime application to removable media, download the application by inserting the removable media in the HMI device and performing the download from the
Settings
screen.
TIP:
Tips:
- When saving the runtime application, the syntax of all expressions, the elements and properties referenced in expressions, and the existence of all project tags in the referenced controller projects are verified.
- IfView Designerencounters a problem, theSave Runtime Applicationwizard indicates that there is an error. Errors appear in theErrorswindow below theView Designerscreen. SelectCloseto close theSave Runtime Applicationwizard and use theErrorswindow to navigate to the source of the error. Resolve all errors before saving the runtime application to removable media.
Provide Feedback