Save a runtime application to removable media
Save a
View Designer
runtime application as a .vpdr file. Files that are a .vpdr file download to the HMI device without using View Designer
. Save the .vpdr file to removable media. After inserting the removable media in the HMI device, download the runtime application to the HMI device.Prerequisites
- To save the runtime application to removable media, insert a USB storage device or SD card into the HMI device.
To save a project to removable media
- SelectFile > Save Project As.WindowsExplorer opens.
- Navigate to the location to save the runtime application.TIP:Save the runtime application directly to a USB drive or SD card, or save the runtime application to another location and then copy the runtime application to the USB drive or SD card.
- In theFile namebox, type a unique name for the runtime application.TIP:Tips:
- Do not insert the characters ( ) or commas in runtime application file names. When selecting a .vpdr file to upload from removable media on the HMI device, any .vpdr file name that contains a comma or ( ) characters does not appear in the list selector. The list selector cannot show file names that contain a comma or ( ).
- If typing the .vpdr extension as part of the file name, type the extension in lowercase letters.
- In theSave as typebox, selectView Designer Runtime Application (.vpdr)and selectSave. TheSave Runtime Applicationwizard opens theSave Runtime Applicationpage. TheLocationbox on theSave Runtime Applicationpage contains the specified location and file name.TIP:Downloading a .vpd project file to the HMI device from removable media is not supported.
- In theDefault language used at startup of HMI device and for undefined translationsbox, select the language in which to display the runtime application on the HMI device.
- SelectSave. The wizard builds and saves the runtime application on the removable device.TIP:Tips:
- While saving, the project is verified. Any warnings and errors that occur appear. SelectCloseand correct any warnings or errors and then save the project again.
- SelectCancelto not save the project.
- When the save is complete, selectClose.TIP:When the runtime application exists in a location other than removable media, copy the .vpdr from the location to the USB drive or SD card.
Provide Feedback