Rename a
View Designer
project file

View Designer
project files can have a different name than the project name. Renaming a project does not rename the project file name.
To rename a
View Designer
project file
  • Use one of the following methods:
    • Navigate to the file location and change the file name. By default, projects are saved as VPD files in the project directory <user>\My Documents\Studio 5000\Projects.
    • Select
      File > Save Project As
      and type a unique name for the project.
      TIP:
      View Designer
      cannot save a .vpd file with a name if a .vpd file of the same name is open in another instance of
      View Designer
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal