Change the HMI device of a project
Change the type of HMI device for a project to change the device for which the project is configured. For example, change the HMI device for a project from a
PanelView
HMI device to a View 5000 Server
. Do this to view the runtime application on the different HMI device. To change the HMI device of a project
- SelectProject > Project Properties. TheTarget HMI Devicedialog box opens.
- Select the HMI device. To search for the HMI device, start typing the name of the HMI device in theSearchbox.
- ClickNext.
- Select the HMI device screen size for aPanelViewHMI device project or the monitor size for aView 5000 Serverproject. The screens in the project represent the physical size of the screen for the project.TIP:Tips:
- The default screen size is for aView 5000 Serverproject isCustom.
- The last configured screen properties appear for the custom screen size. Change the screen properties to specify the unit of measure, screen size,a nd aspect ratio for the screen of aView 5000 Serverproject.
- Changing screen properties automatically selectsCustomas the screen size for aView 5000 Serverproject.
- ClickOK.
Provide Feedback