Add an event command to send an email
Add a command to an event to automatically send an email notification when the event triggers on the HMI device. For example, send an email automatically when a tank reaches or drops below a certain level by adding a
Send email
command to a State Enter or State Exit event. To send an email after pressing a button, add a Send email
command to a touch press event on the graphic element. Prerequisites
- Create an event to automatically trigger the command:
- Touch Press.Occurs when touching the item on the screen that is configured with the event.
- Touch Release.Occurs when releasing the item on the screen that is configured with the event.
- Key Press.Occurs whenpressing the specified key.
- Key release.Occurs when releasing the specified key.
- State Enter.Occurs when a graphic element, screen, popup, or the System Banner transitions into the selected state through an animation.
- State Exit.Occurs when a graphic element, screen, popup, or the System Banner transitions out of the selected state through an animation.IMPORTANT:To send an email when a State Enter or State Exit event triggers, verify that the graphic element, screen, popup, or System Banner is configured forState Tableanimation.
To add an event command to send an email
- Select the graphic element configured with the event.
- In thePropertiespane on theEventstab, selectAdd Command.
- Expand theMessagingcommand category and selectSend email.
- Complete the property boxes on the command card:
- Recipient. The email addresses of the email recipients, separated by commas or semicolons.
- Subject. The subject of the email.
- Message. The complete text of the email to send.
- Status. The status of the sent email in Numeric format (DINT). Status does not support binding to element properties. Bind this property to a controller tag to display the status code of the last email sent by the command:
- Successfully sent: 10. This code indicates the email was successfully sent to all recipients.
- Error returned from email server: 20. This code indicates multiple errors such as a timeout while sending the email, an incorrect email address, or a communication error with the email server.
- Unable to reach email server: 30. This code indicates multiple errors such as an invalid password, invalid user name, or invalid server name.
- Sending is in progress (email added to queue): 40. This code indicates an email is in progress to a recipient.
- Email request rejected: 50. This code indicates the maximum buffer size of 120 email requests are in queue. Decrease the number of email commands that execute simultaneously.TIP:Tips:
- Manually enter values in the property boxes to send a pre-configured static message when the event triggers. Use this method when sending only one or two emails and when entering information directly in the command is preferred.
- To send a large number of emails with updated information from the system when the event triggers, bind the property boxes to tags in a controller.
Provide Feedback