Add an event command to reboot the HMI device
Add an event command to reboot the HMI device. Rebooting the HMI device is also performed through the Settings screen on the HMI device.
Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs whenpressing the specified key.
- Key release.Occurs when releasing the specified key.
- Expand the
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
HMI Device Configurationcategory and selectReboot Terminal.
Provide Feedback