Add an event command to close the web browser
Create an event command to close the web browser.
IMPORTANT:
The
PanelView
53xx family of HMI devices does not support the web browser.Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs whenpressing the specified key.
- Key release.Occurs when releasing the specified key.
- Expand the
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
Navigationcategory, and then selectClose Web Browser.
Provide Feedback