Add an event command to clear one or more data logs
Create an event to clear data logs. Add a clear data log command to clear one or more data logs, or all data logs at once.
Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs whenpressing the specified key.
- Key release.Occurs when releasing the specified key.
- Expand the
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
Data Logcategory and select and configure the command:
- Data Log. SelectAll data logsor select a specific data log name.
- Status
- Data log clearing in progress: 10.
- Data log successfully cleared: 20.
- Unable to clear data log. Data log is not configured: 30.
- Unable to clear data log. Data log is not running: 40.
- Selected data log does not exist: 50.
- Clear data log command is already in progress: 60.
- Unable to clear data log. Export is in progress: 70.
- Unable to clear data log. Insert SD card: 80.
- Unable to restart the cleared data log. Remove and replace the SD card: 90.
- Unable to clear the data log. Try again or restart terminal: 100.
- Configure another command to clear additional data logs.
Provide Feedback