Rename a project event

Rename a project event to reflect the purpose, content, or targeted use of the event. Names within a folder must be unique and are not case sensitive. For example, Monthly_ProjectEvent and monthly_projectevent are considered identical names.
To rename a project event
  1. In the
    Project Explorer
    , expand the
    Project Events
    folder.
  2. Click the project event once to select the item.
  3. Click the project event again and type the new name.
    TIP:
    Tips:
    • Rename a project event by right-clicking the name and clicking
      Rename
      . Then type a new name and press
      Enter
      .
    • Change the name of the project event through the
      Name
      box in the
      Properties
      window of the project event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal