Delete a project event
Delete a project event to no longer have the event evaluated and triggered. Deleting an event from the
Project Events
folder:- Removes the project event from the folder
- Clears the ProjectEventName property in thePropertiestab for each project event that references the ProjectEventName.
To delete a project event
- In theProject Explorer, open theAssets > ProjectEventsfolder.
- Right-click the project event and clickDelete.
Provide Feedback