Copy a project event between projects
Copy a project event between
View Designer
projects to ensure consistency.Prerequisites
- Open the sourceView Designerproject containing the content to copy.
- If the content is to be pasted into another project, for each project, start an instance ofView Designerand open the target project. It is recommended to open no more than three instances ofView Designerat one time.
To copy a project event between projects
- Copy the project event from the source folder to the targetProject Eventsfolder.
- If the target project contains a project event with the same name:
- ClickReplaceto overwrite the existing file.
- ClickKeep bothto rename the project event copied from the source folder
- ClickCancelto not copy the the project event.
Provide Feedback