Breadcrumb navigation in the Tag Browser and the Data Type Browser
Tag Browser
and the Data Type Browser
Use breadcrumbs in the and the to identify the location in the browser hierarchy and to navigate to other levels. Each level accessed is added to the breadcrumb. Breadcrumb navigation includes:
Tag Browser
Data Type Browser
To do this: | Do this: |
Access a level. | Select any level except the last. |
Return to the highest level of the hierarchy. | Select Home |
Open a list of sub-levels. | Select the single arrow |
Return to a recently browsed path. | Select the double arrow or |
TIP:
If a breadcrumb is too long to fit in the window, the window displays a double arrow. A double arrow indicates there is more content to the left or to the right of the current location in the breadcrumb.
Provide Feedback
or